E

Triangulation LIDAR

RPLIDAR A1

Basic model

RPLIDAR A2

Cost effective

RPLIDAR A3

Multipoint interaction
E

TOF LIDAR

LPX-T1

AGV preferred

RPLIDAR S2

Indoor & Outdoor

RPLIDAR S3

Best performance in black objects

RPLIDAR C1

The newest model
E

Mapping Solution

Mapper M2

M2M2 Mapper

Slamkit

SLAM spatial localization
E

Robot Base

Hermes

Max loadweight 80KGS

Athena 2.0

Compact and flexible

Apollo

Autonomous Navigation
E

Robot

F3

food delivery robot

H2

hotel robot

P3 PRO

factory robot
E

Discount

  • SLAMTEC Blog
Techno Blog from Slamtec

RPLIDAR A3: Advanced Triangulation LiDAR for Extended Range and Reliability

RPLIDAR A3: Advanced Triangulation LiDAR for Extended Range and Reliability

The RPLIDAR A3M1 is a low-cost 360-degree 2D laser scanner (LIDAR) solution developed by SLAMTEC. Collects up to 16,000 laser samples per second ranging at high rotational speeds. It is also equipped with SLAMTEC’s patented OPTMAG technology, which breaks through the life limit of traditional lidar and enables the system to work stably for a long time.

Hermes Debuts in Singapore Milipol Asia-Pacific Adorned in Blue Battle Armor, Empowering Smart Security

Hermes Debuts in Singapore Milipol Asia-Pacific Adorned in Blue Battle Armor, Empowering Smart Security

On April 5, 2024, the 10th edition of Milipol Asia-Pacific, the International Exhibition of Military and Police Forces, concluded at the Sands Expo & Convention Centre in Singapore. Hundreds of exhibitors from around the world showcased the latest security, anti-terrorism, and criminal investigation technologies, solutions, and related products, empowering new international methods in security and counter-terrorism.

SLAMTEC’s Huang Jueshen: Enabling Robots to ‘See’ Clearly and Move More Intelligently

SLAMTEC’s Huang Jueshen: Enabling Robots to ‘See’ Clearly and Move More Intelligently

Introduction: Digitization and intelligentization are comprehensively reshaping industrial production processes, leading to the emergence of numerous dark horse enterprises in the field of intelligent manufacturing. Driven by the combined demands of industry and robotics, the application market for LiDAR, a sensing hardware terminal, demonstrates a potential market value exceeding hundreds of billions of yuan.

【Tutorial】Introduction Guide to SLAMWARE ROS SDK

【Tutorial】Introduction Guide to SLAMWARE ROS SDK

ROS, as one of the most widely used infrastructures in the robotics industry, is the preferred framework for many users developing robot applications. If you want to integrate SLAMWARE’s robot chassis or SLAMKit mapping and localization solutions into a system developed based on ROS, what is the most convenient method? ROS SDK is designed for this purpose. This article will introduce you to the basic architecture, deployment methods, and application examples of ROS SDK.

Common Questions and Answers about SLAMTEC Products

Common Questions and Answers about SLAMTEC Products

一.RPLIDAR

Q: Why can’t the radar connect?

A: Please check if the corresponding USB option is selected correctly. When adding a radar connection, make sure to choose the correct COM port. For example, if you’ve plugged in a radar and it has been assigned COM4, then select COM4 in the USB options, and proceed with the connection startup.

Capturing Environmental Details Quickly with a More ‘Intelligent’ Lidar

Capturing Environmental Details Quickly with a More ‘Intelligent’ Lidar

In recent years, the rapid advancement of low-speed unmanned driving applications in specific scenarios has been observed. The maturity of lidar, serving as a core sensor, is crucial for the practical implementation of low-speed unmanned driving. Moreover, compared to radar products used in autonomous vehicles, lidar products have higher requirements for detecting environmental details.

The Application of SLAMTEC LiDAR Sensors

The Application of SLAMTEC LiDAR Sensors

SLAMTEC is a company dedicated to the research and production of LiDAR technology. LiDAR sensors utilize laser beams to measure distances to targets and generate high-resolution maps. They find wide applications across various sectors including catering, hospitality, government affairs, business, education, healthcare, among others, helping businesses reduce costs and increase efficiency. Below are some application areas of SLAMTEC LiDAR sensors.

The outstanding application of RPLIDAR A1 in robotic vacuum cleaners

The outstanding application of RPLIDAR A1 in robotic vacuum cleaners

In the realm of smart homes, robotic vacuum cleaners are becoming an indispensable part of modern living. To enhance the environmental perception and navigation performance of these devices, Slamtec Technology has introduced the RPLIDAR A1, a laser radar product that incorporates advanced laser radar technology, providing exceptional environmental perception and navigation capabilities for robotic vacuum cleaners.

SLAMTEC Athena 2.0: The Outstanding Evolution of Intelligent Elevator Control Systems

SLAMTEC Athena 2.0: The Outstanding Evolution of Intelligent Elevator Control Systems

Athena 2.0 is a small, scalable, and cost-effective robotic platform developed by SLAMTEC, designed to meet the development needs of small-scale robot applications. These applications include intelligent inspection robots, cargo transport robots, restaurant delivery robots, and more. It comes equipped with SLAMTEC’s latest upgraded high-performance SLAMCUBE2 autonomous navigation and positioning system, enabling it to perform path planning and location navigation. This capability allows Athena 2.0 to operate in various commercial environments, supporting the integration of different applications.

SLAMTEC Mapper Quick Start Guide

SLAMTEC Mapper Quick Start Guide

SLAMTEC Mapper operates on the unique SLAM optimization algorithm developed by Slamtec, combined with a high-performance laser radar. It can perform map data fusion over 10 times per second and generate maps for areas up to 100,000 square meters. The laser radar conducts distance measurements at a rate of 9,200 times per second, with a maximum range of 40 meters. Real-time data processing is carried out by the built-in processing system, delivering high-precision mapping and positioning information

SLAMTEC RPLIDAR S2: High-Speed Obstacle Avoidance LiDAR, 30-Meter Omnidirectional Range Scanning

SLAMTEC RPLIDAR S2: High-Speed Obstacle Avoidance LiDAR, 30-Meter Omnidirectional Range Scanning

A service robot deployed in office buildings, factories, hotels, hospitals, and similar environments requires autonomous mobility and obstacle avoidance capabilities. To achieve obstacle avoidance in unknown environments, laser radar sensors are commonly employed. These sensors provide accurate environmental information, including obstacle dimensions and positions, enabling the robot to dynamically adjust its path, move safely, and accomplish tasks in real-time.

Deployment and Usage Instructions for SLAMTEC Hermes

Deployment and Usage Instructions for SLAMTEC Hermes

Hermes is a medium-sized, scalable, and cost-effective robotic platform developed by SLAMTEC to meet the needs of small and medium-sized robot application development. Applications include intelligent inspection robots, container transport robots, hotel delivery robots, restaurant food delivery robots, and more.

Quick Start Guide for RPLIDAR LPX-T1

Quick Start Guide for RPLIDAR LPX-T1

LPX-T1 is a new generation long and medium-range high-performance laser radar developed by SLAMTEC. It boasts a ranging capability of up to 40 meters, with a rapid laser ranging sampling rate of up to 60,000 times per second. Additionally, it exhibits strong resistance to ambient light, with a capability of up to 80,000 lux. The scanning angle covers 270 degrees, allowing it to generate real-time planar point cloud map information, providing precise environmental perception and navigation support.

SLAMTEC Mapper Mapping and Localization Radar

SLAMTEC Mapper Mapping and Localization Radar

SLAMTEC Mapper is a new category of laser sensor introduced by SLAMTEC, distinct from traditional lidar sensors. This product comes equipped with SLAM real-time mapping and localization capabilities, suitable for various applications such as robot navigation, environmental mapping, and handheld measurements.