主页
产品 产品
新闻动态
购买渠道
下载与支持
关于我们
加入我们
联系我们
  • 中文 |
  • Eng
  • news title separator Lidar vs. Millimeter-Wave Radar: What’s the Difference?

    Radar sensors are essential for environmental perception in robotics, autonomous driving, and smart devices. Among them, the two most commonly discussed technologies are Lidar (Light Detection and Ranging) and millimeter-wave radar (MMW radar).

    At first glance, both systems seem similar: they detect objects by sending out signals and analyzing the reflected waves. But in practice, Lidar and millimeter-wave radar work very differently, and each has unique strengths and weaknesses.

    This guide explains the key differences between Lidar and millimeter-wave radar in terms of working principle, accuracy, resistance to interference, and cost.

    1. Working Principle

    • Lidar (Laser Radar):
      Uses laser beams (light particles) to measure distance, position, and velocity of objects. The emitted beam travels in a straight line, and reflections are collected to create detailed images and maps of the environment.

    • Millimeter-Wave Radar:
      Operates in the millimeter-wave frequency band—higher than radio waves but lower than visible light and infrared. Instead of straight-line beams, it sends out a cone-shaped electromagnetic wave. The antenna relies on electromagnetic radiation to detect reflections.

    👉 In simple terms: Lidar works like human vision (straight-line detection), while millimeter-wave radar is more like bat echolocation, using broader signals to detect surroundings.

    2. Detection Accuracy

    • Lidar: Known for high precision, wide detection range, and strong stability. It can accurately model the environment, detect pedestrians, and identify small obstacles with fine detail.

    • Millimeter-Wave Radar: Limited by frequency loss. To achieve longer detection ranges, higher frequency radars are required, but these still cannot match Lidar’s accuracy. Millimeter-wave radar struggles to model surrounding obstacles with precision and cannot reliably detect pedestrians.

    👉 Winner: Lidar – offers far greater accuracy and mapping capabilities.

    3. Resistance to Interference

    • Lidar: Sensitive to environmental conditions. Rain, snow, fog, or dust can block the light beams, making the sensor unreliable in harsh weather.

    • Millimeter-Wave Radar: Has strong penetration through fog, smoke, and dust. It works well in bad weather conditions where Lidar cannot function.

    👉 Winner: Millimeter-Wave Radar – much more robust in adverse environments.

    4. Cost and Processing Power

    • Lidar: Provides large amounts of detailed data, which requires powerful processors to handle. This makes Lidar systems more expensive overall.

    • Millimeter-Wave Radar: Simpler data output, easier to process, and generally more cost-effective.

    👉 Winner: Millimeter-Wave Radar – cheaper and less demanding, but less precise.

    5. Which is Better Overall?

    • Lidar: Best choice for applications where high accuracy, precise obstacle detection, and detailed mapping are required. This is why Lidar is popular in autonomous vehicles, robotics, and mapping systems.

    • Millimeter-Wave Radar: More reliable in bad weather and cost-sensitive projects, making it useful as a complementary sensor for vehicles and drones.

    Conclusion:

    While both sensors have their place, Lidar is generally superior in performance and accuracy, though millimeter-wave radar remains valuable for weather resistance and cost efficiency. In practice, many advanced systems use a fusion of Lidar and millimeter-wave radar to take advantage of both technologies.

    Keywords: rplidar, slam, technology guide

    top
    FaceTime Icon