主页
产品 产品
新闻动态
购买渠道
下载与支持
关于我们
加入我们
联系我们
  • 中文 |
  • Eng
  • news title separator Common Indoor SLAM Failure Scenarios and How to Fix Them

    Why Indoor Localization and Navigation Still Fail in Real Deployments

    Indoor mobile robots are now widely used in home, commercial, service, and industrial environments. With the help of SLAM-based localization and navigation systems, robots can autonomously move, build maps, and plan paths in structured indoor spaces.
    However, during real-world deployment, robots often encounter environmental conditions that significantly degrade localization accuracy or mapping quality. These issues are especially common in 2D LiDAR-based indoor navigation systems and are not always obvious during initial testing.
    In this article, we examine several common indoor failure scenarios and provide practical, field-proven solutions to improve SLAM robustness and navigation performance.

    Scenario 1: Glass, Mirrors, and Highly Reflective Surfaces

    Why This Causes Problems

    Glass walls, mirrors, polished surfaces, and smooth reflective materials are among the most challenging environments for 2D LiDAR-based robots.
    LiDAR relies on laser pulses reflecting back from surrounding objects. However, specular reflection occurs when laser beams hit smooth or transparent surfaces. Instead of returning to the receiver, the laser is reflected away, causing:
    • Missing distance measurements
    • Incomplete map structures
    • Localization drift or sudden jumps
    Over time, these effects can lead to unstable SLAM performance and navigation failures.
    Highly Reflective Surfaces

    Practical Solutions

    To improve LiDAR detectability in reflective environments, the following methods are commonly used:
    1. Apply Frosted or Matte Treatment

    Directly applying a frosted finish to reflective surfaces can significantly improve laser reflection quality, increasing the effective detection range and measurement stability.
    Apply Frosted or Matte Treatment
    1. Use High-Reflectivity Matte Tape

    Applying standard high-reflectivity matte tape to the surface can greatly reduce measurement loss. This method is simple, low-cost, and highly effective in most indoor environments.
    Use High-Reflectivity Matte Tape
    1. Attach Frosted Film (Short-Range Use)

    Frosted films can also improve LiDAR performance, but this solution is typically effective only at shorter distances (approximately within 3 meters).
    Attach Frosted Film
    1. Use Printed or Textured Adhesive Materials

    Advertising-grade printed adhesive tapes or textured materials can help extend the measurable range by introducing surface irregularities that improve laser return signals.
    printed adhesive material

    Scenario 2: Long Corridors With No Distinct Features

    Why This Causes Problems

    Long corridors—such as those found in hotels, shopping malls, and office buildings—often lack distinct geometric features. From a SLAM perspective, these environments are highly repetitive and symmetric.
    As a result:
    • Consecutive LiDAR scans appear nearly identical
    • Scan matching becomes ambiguous
    • Localization error accumulates over long distances
    • Maps may stretch, drift, or collapse
    This is a classic failure mode for SLAM systems that rely on geometric consistency and feature diversity.
    Long Corridors

    Practical Solutions

    1. Introduce Physical Features Into the Environment

    Placing objects such as potted plants along the corridor can significantly improve localization stability. These objects introduce unique spatial features that help SLAM algorithms distinguish between different corridor segments.
    Recommendation: Use pots with matte, high-reflectivity surfaces to ensure reliable LiDAR detection.
    Introduce Physical Features Into the Environment
    1. Feature the Corridor Side Walls

    If the corridor side walls are detectable by LiDAR, a simple and effective approach is to introduce periodic non-detectable regions:
    • Add a black decorative strip or non-reflective area
    • Place one segment approximately every 3–4 meters
    • Each segment can be around 30 cm in length
    These intentional interruptions help create distinguishable patterns in LiDAR scans, improving scan matching and localization accuracy.
    1. Modify Non-Detectable Walls Before Feature Placement

    If the corridor walls are initially non-detectable (e.g., glass or smooth reflective surfaces):
    1. First apply one of the reflective-surface treatments described in Scenario 1
    2. Then introduce periodic non-detectable segments as described above
    The layout does not need to be perfectly uniform. As long as distinctive features appear at regular intervals, SLAM performance will improve significantly.

    System-Level Perspective: Designing SLAM-Friendly Environments

    These scenarios highlight an important but often overlooked fact:
    Reliable indoor localization is not only a software problem—it is also an environmental design problem.
    For 2D LiDAR-based indoor robots, SLAM performance depends heavily on:
    • Stable geometric features
    • Consistent laser reflections
    • Sufficient environmental variation
    By making small, low-cost adjustments to the physical environment, it is often possible to achieve dramatic improvements in localization and navigation reliability without changing hardware or algorithms.

    Where These Issues Most Commonly Occur

    The challenges discussed in this article are especially common in:
    • Delivery and cleaning robots
    • Inspection and patrol robots
    • Environments such as hotels, malls, hospitals, and office buildings
    They are particularly relevant for systems based on 2D LiDAR, wheel odometry, and SLAM-based localization.
    rplidar s3 in complex enviroment

    Conclusion

    SLAM-based indoor navigation performs well in many environments, but certain real-world conditions—such as reflective surfaces and featureless corridors—can severely impact accuracy and stability.
    By understanding why these failures occur and applying simple, practical environmental modifications, system integrators and robot developers can greatly enhance localization robustness and overall navigation performance.
    These engineering-focused adjustments are often the key difference between a system that works in testing and one that performs reliably in real-world deployment.

    关键字:SLAM,Technology Explained

    top
    FaceTime Icon