主页
产品 产品
新闻动态
购买渠道
下载与支持
关于我们
加入我们
联系我们
  • 中文 |
  • Eng
  • news title separator What Really Matters When Choosing a 2D LiDAR for Mobile Robots

    Why LiDAR Specifications Alone Don't Guarantee Real-World Performance

    When selecting a 2D LiDAR for mobile robots, many engineers instinctively focus on familiar specifications such as maximum range, scanning frequency, and distance accuracy.
    While these parameters are important, they represent only part of the picture. In real-world indoor deployments, many robots fail not because their LiDAR lacks range or precision, but because it performs poorly under challenging environmental conditions.
    Two often-overlooked factors play a critical role in determining whether a LiDAR is truly practical and reliable:
    • Resistance to strong ambient light
    • Detection capability for dark, low-reflectivity objects
    These characteristics can make or break a robot's localization and navigation performance.

    Range Is Important — But Context Matters

    Distance measurement is the core function of any LiDAR sensor, so maximum detection range naturally receives the most attention. However, focusing solely on the advertised maximum range can be misleading.
    In addition to maximum range, practical deployment depends on:
    • Angular resolution
    • Scan frequency
    • Sampling rate
    • Measurement consistency across distances
    These factors directly affect map quality, localization stability, and maximum robot speed.

    Scan Frequency vs. Sampling Rate: A Common Misunderstanding

    Higher scan frequency allows a robot to move faster while maintaining stable SLAM performance. However, increasing scan speed is not as simple as rotating the internal motor faster.
    If the sampling rate does not increase accordingly, higher scan speeds will reduce angular resolution. This leads to:
    • Sparse point clouds
    • Poor feature extraction
    • Degraded scan matching accuracy
    In practice, scan frequency and sampling rate must be balanced at the system level to ensure reliable perception at higher robot speeds.
    S3 sampling diagram

    Accuracy and Resolution at Long Distances

    Most 2D LiDAR systems achieve high distance resolution within short ranges (typically under 10 meters). However, due to physical measurement principles, resolution and accuracy degrade rapidly as distance increases.
    Extending effective detection range requires more than simply increasing laser power. It demands:
    • Fundamental improvements in ranging algorithms
    • Optimized signal processing pipelines
    • Careful hardware–software co-design
    • Manufacturing-level consistency for mass production
    This is where many LiDAR designs struggle to scale beyond laboratory performance.

    Why Dark Object Detection Matters More Than You Think

    In real indoor environments, walls are rarely perfect white surfaces. Robots must navigate around:
    • Dark furniture
    • Black-painted walls
    • Low-reflectivity materials
    • Textured or absorbent surfaces
    If a LiDAR detects white walls at 10 meters but can only detect dark objects at 2–3 meters, SLAM and navigation will inevitably fail.
    Poor dark-object detection leads to:
    • Incomplete maps
    • Localization drift
    • Missed obstacles
    • Unsafe navigation behavior
    Yet this performance metric is rarely highlighted in standard datasheets.
    RPLIDAR S3 designed for complex actual enviroment

    The Problem With Reflectivity-Based Range Claims

    Most LiDAR manufacturers specify detection range based on 90% reflectivity diffuse targets, such as white paper. While this provides a standardized benchmark, it does not reflect real-world conditions.
    Dark objects absorb most of the emitted laser energy. Achieving the same detection range for low-reflectivity surfaces is extremely challenging—especially for triangulation-based LiDAR systems, which rely heavily on reflected signal strength.
    As a result, effective detection range on dark targets is often a far more meaningful metric than maximum range under ideal conditions.

    Advancements in Dark Object Detection With RPLIDAR S3

    Detecting dark, low-reflectivity objects has long been one of the most challenging problems in 2D LiDAR design. In real indoor environments, robots frequently encounter black furniture, dark walls, and low-reflectivity materials, all of which absorb most of the emitted laser energy.
    RPLIDAR S3 is designed specifically to address this challenge at the product level. Even when facing targets with only 10% reflectivity, the sensor is able to achieve a stable detection range of up to 15 meters, ensuring that dark objects remain visible to the robot's perception system.
    At the same time, RPLIDAR S3 maintains a non-degrading measurement radius of up to 40 meters at 70% reflectivity, avoiding the common issue where advertised long-range performance collapses under real-world conditions. This balanced performance across both high- and low-reflectivity targets is critical for reliable SLAM, mapping continuity, and obstacle detection.
    Rather than optimizing for ideal laboratory targets, the ranging performance of RPLIDAR S3 is engineered for real indoor robot environments, where surface materials and reflectivity vary significantly.
    rplidar s3 banner

    Designing LiDAR for Real Indoor Robots: The RPLIDAR S3 Approach

    For indoor mobile robots, LiDAR performance must remain reliable under a wide range of operating conditions. This includes not only object reflectivity, but also ambient light, robot speed, and physical integration constraints.
    RPLIDAR S3 delivers a high-speed sampling rate of up to 32,000 samples per second, providing dense point cloud data for real-time perception. This enables:
    • Faster and more accurate map construction
    • Improved localization stability at higher robot speeds
    • More reliable detection of small or fast-changing obstacles
    In environments with strong lighting, LiDAR sensors often suffer from reduced signal quality. Thanks to hardware-level optimization, RPLIDAR S3 offers ambient light resistance up to 80 KLux, allowing it to operate reliably under indoor strong lighting as well as outdoor sunlight exposure without compromising ranging accuracy.
    From a mechanical integration perspective, RPLIDAR S3 is designed to fit seamlessly into modern robot platforms. With a compact and slim form factor—only 4 cm in height—it enables flexible integration in space-constrained designs while delivering strong overall performance.
    rplidar s3 height
    By combining long-range stability, low-reflectivity detection, high sampling speed, and strong ambient light resistance in a compact package, RPLIDAR S3 is well suited for indoor mobile robots that require dependable SLAM, localization, and navigation performance in real-world deployments.

    Conclusion

    Choosing a 2D LiDAR for mobile robots is not just about range, accuracy, or scan frequency. True reliability depends on how the sensor performs in non-ideal, real-world conditions.
    Key factors such as ambient light resistance and dark object detection capability are essential for robust SLAM and navigation—but are often overlooked.
    For engineers and system integrators, understanding these hidden performance metrics is critical to building mobile robots that work reliably beyond controlled test environments.

    关键字:Lidar,Technology Explained

    top
    FaceTime Icon