In modern robotics, SLAM (Simultaneous Localization and Mapping) plays a fundamental role in enabling machines to understand and interact with their environment. However, a common misconception is:
SLAM = autonomous navigation
This is not accurate.
While SLAM is essential, it represents only one part of a much larger system. To understand why, we need to look at what SLAM does—and what it does not do.
What SLAM Actually Solves
SLAM focuses on two core problems:
In simple terms, SLAM answers:
"Where am I, and what does the world around me look like?"
This capability is critical, but it does not tell the robot:
These tasks belong to navigation, not SLAM.
What Is Autonomous Navigation?
Autonomous navigation is the process that enables a robot to move from point A to point B safely and efficiently.
A more complete representation is:
Autonomous Navigation = SLAM + Path Planning + Motion Control
After SLAM provides the robot’s position and a map, the system must:
1.Plan a path to the target
2.Adjust the path in real time when conditions change
3.Execute motion commands to follow that path
Without these additional components, a robot can "see" the world but cannot act intelligently within it.
Global vs. Local Path Planning
Path planning is typically divided into two layers:
Global Planning
Global planning operates on a known or partially known map. It computes an optimal path from the robot's current position to the goal.
Works best in static environments
Focuses on efficiency and optimality
Local Planning
Local planning operates in real time and handles:
It does not necessarily know the final goal in detail, but it is highly effective at:
"How do I safely move forward right now?"
From Classic to Modern Path Planning Algorithms
Early discussions of robot navigation often begin with classical algorithms such as A* and D*. These methods form the theoretical foundation of many modern planning systems and are still widely used today.
A* (A-Star) Algorithm — Optimal Path in Static Environments
A* is one of the most well-known path planning algorithms for finding the shortest path in a graph or grid-based map.
It works by minimizing a cost function:
The total cost is:
f(n) = g(n) + h(n)
The algorithm continuously explores nodes with the lowest estimated total cost, gradually approaching the optimal path.
Key characteristics of A*:
-
Guarantees the shortest path (if the heuristic is admissible)
-
Highly efficient in static or known environments
-
Performance depends heavily on the quality of the heuristic function
Limitations:
-
Assumes the environment does not change
-
If obstacles appear, the path must be recomputed from scratch
This makes A* ideal for:

D* (Dynamic A-Star) Algorithm — Adaptive Planning in Changing Environments
D* (Dynamic A*) extends A* to handle unknown or dynamically changing environments.
Instead of computing a path once, D* is designed to:
Continuously update the path as new information becomes available.
When the robot detects changes—such as newly discovered obstacles—it does not restart the entire planning process. Instead, it incrementally repairs the existing path.
Key characteristics of D*:
-
Supports real-time replanning
-
Efficiently updates only the affected parts of the path
-
Suitable for partially known or unknown environments
Why D* matters:
Compared to A*, D* allows robots to behave more like humans:
Start moving with partial knowledge, and adjust the route as the environment becomes clearer.
Common variants:
Commonly Used Modern Planning Algorithms
1.DWA (Dynamic Window Approach)
2.TEB (Timed Elastic Band)
-
Optimizes trajectories over time
-
Balances path smoothness, safety, and efficiency
3.RRT / RRT*
4.MPC (Model Predictive Control)
These algorithms highlight an important reality:
Navigation is not just about finding a path—it is about continuously optimizing movement under real-world constraints.
Navigation Is Not One-Size-Fits-All
Different types of robots require fundamentally different navigation strategies. This is another reason why SLAM alone cannot define "intelligent navigation."
1.Cleaning Robots (Coverage First)
For robot vacuums, the goal is not simply reaching a destination.
Instead, they must:
This leads to Coverage Path Planning (CPP) techniques, such as:
The objective is: cover everything, not just go somewhere.
2.Warehouse Robots/AMRs (Efficiency First)
Autonomous Mobile Robots (AMRs) prioritize:
Here, path planning focuses on:

3.Autonomous Driving (Safety First)
Autonomous vehicles operate in highly dynamic and unpredictable environments.
Key requirements include:
-
Predicting human behavior
-
Handling complex traffic scenarios
-
Ensuring strict safety constraints
Navigation here goes far beyond SLAM and basic planning—it involves:
4.Humanoid and Service Robots (Understanding First)
Emerging robots, especially in embodied intelligence, require:
This shifts navigation toward:
In response to this situation, SLAMTEC has released its next-generation fully integrated AI spatial perception system—
Aurora S. A good pair of eyes needs to see widely, understand the environment, and be resistant to strong light, reflections, and mirrors. This is why Aurora S is so popular with many embodied companies!
Coverage Planning: A Special Case of Navigation
Unlike standard navigation tasks, some robots must cover an entire area, not just move between two points.
This is especially important in:
-
Cleaning robots
-
Inspection robots
-
Agricultural robots
Key challenges include:
This is why coverage planning is considered a distinct research field within robotics.
Conclusion: SLAM Is the Foundation, Not the Whole System
SLAM is a critical enabling technology, but it is only one component of autonomous navigation.
A fully functional navigation system requires:
-
Environmental perception (SLAM)
-
Intelligent planning (global + local)
-
Real-time control and execution
Most importantly:
Different applications demand different navigation strategies.
As robotics continues to evolve, navigation systems are becoming more integrated, combining perception, planning, and intelligence into unified frameworks.
But one principle remains unchanged:
No matter how advanced SLAM becomes, it does not replace the need for planning and control.