主页
产品 产品
新闻动态
购买渠道
下载与支持
关于我们
加入我们
联系我们
  • 中文 |
  • Eng
  • news title separator How Service Robots Navigate Indoors: From SLAM to Path Planning

    Why Autonomous Navigation Is Critical for Service Robots

    For service robots to move freely in indoor environments, autonomous localization and navigation are essential capabilities. Autonomous navigation typically consists of three core components: localization, mapping, and path planning.
    SLAM (Simultaneous Localization and Mapping) has become the backbone technology for indoor robot navigation and has gained widespread attention across the robotics industry. However, SLAM alone does not fully equal autonomous navigation. In real-world applications, SLAM focuses on localization and map creation, while navigation also requires robust motion and path planning.
    So how does SLAM actually work in practice? And what are the key challenges when deploying it in real service robots?

    Why Indoor Robots Need Maps

    When humans get lost, digital maps and navigation apps become our most reliable tools. Service robots are no different. To understand and interact with their environment, robots rely on maps to represent the surrounding space.
    Depending on sensor configuration and algorithm design, robots may use different map representations. Among them, occupancy grid maps are the most widely used in indoor mobile robots today.
    occupancy grid maps

    Occupancy Grid Maps Explained

    An occupancy grid map divides the environment into a large number of small grid cells. Each cell stores a probability indicating whether that space is occupied by an obstacle.
    Conceptually, this type of map resembles a standard 2D image, but instead of visual color values, each "pixel" represents the likelihood of physical occupancy in the real world. This idea was first proposed by Alberto Elfes at NASA in 1989 and was even applied in early Mars rover projects.
    Occupancy grid maps are especially suitable for SLAM systems based on 2D LiDAR, depth cameras, ultrasonic sensors, and other distance-measuring sensors. Today, 2D LiDAR has become the dominant sensor for building such maps in indoor service robots.

    How SLAM Works in Real Systems

    A complete SLAM and navigation system typically follows a structured processing pipeline.
    At its core, SLAM consists of three main steps.
    slam mapping flow diagram
    A standard SLAM System flow

    1.Sensor Data Preprocessing

    A LiDAR sensor captures only a partial snapshot of the environment at any given moment, producing what is commonly known as a point cloud. Raw sensor data often contains noise, missing points, or measurement errors.
    The preprocessing stage filters and optimizes this raw data to improve reliability before further computation.
    lidar point cloudlidar point cloud

    2.Scan Matching

    The second and most critical step is matching—aligning the current LiDAR scan with the existing map to determine the robot's position.
    Algorithms such as ICP (Iterative Closest Point) are commonly used to match point clouds. This process is often compared to solving a puzzle: the system must determine where the new piece best fits within the existing picture.
    The accuracy of scan matching directly determines the quality of localization and map construction. Without proper matching, the generated map quickly becomes distorted and unusable.
    map without matching
    map without scan matching

    3.Map Fusion and Update

    After matching, new sensor data must be fused into the global map. This is not a simple overlay process. Real-world environments are dynamic—people move, objects appear or disappear, and sensors inevitably introduce uncertainty.
    As a result, SLAM systems rely heavily on probabilistic methods and filtering techniques to continuously update the map while accounting for uncertainty and noise.
    This fusion process runs continuously throughout the SLAM operation and gradually produces a stable occupancy grid map.
    slam map fusion flow
    slam map fusion flow

    Key Challenges in Practical SLAM Deployment

    Although the SLAM workflow appears straightforward in theory, real-world deployment introduces significant challenges.

    Loop Closure

    One of the most well-known challenges is loop closure. When a robot travels around a large environment and returns to a previously visited location, accumulated localization errors may prevent the map from closing correctly, resulting in visible distortions.
    Loop closure errors often remain undetected until the robot completes a full loop, at which point correcting the map becomes extremely difficult. A commercial-grade SLAM system is often judged by how robustly it handles loop closure in large-scale environments.
    normal completed mapnormal completed map
    map without loop closure
    map without loop closure

    Environmental Interference

    Another challenge is external interference. Since 2D LiDAR is typically mounted close to the robot chassis, its field of view is limited. Moving obstacles such as people or pets can significantly disrupt localization accuracy and mapping stability.
    Handling these dynamic factors requires extensive system-level optimization beyond basic SLAM algorithms.

    Computational Constraints

    SLAM is computationally intensive. In addition to LiDAR data, it often requires support from IMU and wheel odometry to maintain accuracy.
    Many service robots—such as robotic vacuum cleaners—cannot afford PC-level computing hardware. Making SLAM run reliably on embedded systems requires substantial algorithm optimization and system integration.

    From SLAM to Navigation: The Role of Path Planning

    While SLAM provides localization and maps, navigation requires motion planning, which SLAM alone does not handle.
    Motion planning determines how a robot moves from point A to point B and is typically divided into two layers:

    Global Planning

    Global planning computes an overall route based on the known map and the robot's current position. Algorithms such as A* are widely used for this purpose due to their efficiency and reliability.

    Local Planning

    Local planning handles real-time obstacle avoidance. It allows the robot to react dynamically to unexpected obstacles without recalculating the entire global path.
    Both layers must work together to enable smooth and reliable indoor navigation.

    Advanced Path Planning for Service Robots

    In real environments, static planning is often insufficient. Robots must adapt to unknown or changing conditions.
    Dynamic planning algorithms, such as improved D* variants, allow robots to explore unknown environments while continuously adjusting their paths. These algorithms have even been used in planetary exploration missions.
    For robotic vacuum cleaners and similar service robots, navigation requirements go even further. Functions such as edge cleaning, systematic coverage, and autonomous recharging demand specialized coverage planning algorithms.
    Research in this area is commonly referred to as space coverage, with methods such as Morse decomposition enabling efficient area partitioning and cleaning strategies.

    Bringing It All Together in Commercial Systems

    Transforming SLAM and navigation algorithms into reliable commercial products requires far more than academic research. It involves extensive handling of corner cases, sensor fusion, parameter tuning, and system-level optimization.
    For service robot manufacturers, integrating SLAM, localization, and path planning into a compact and energy-efficient solution is a critical engineering challenge.

    Final Thoughts

    Autonomous navigation in service robots is the result of close cooperation between SLAM, localization, and motion planning. While SLAM forms the foundation, real-world deployment depends on robust system design and practical engineering solutions.
    As indoor service robots continue to evolve, mature and optimized SLAM-based navigation systems will remain a key enabler of scalable and reliable autonomous movement.

    关键字:SLAM,Technology Explained

    top
    FaceTime Icon