主页
产品 产品
新闻动态
购买渠道
下载与支持
关于我们
加入我们
联系我们
  • 中文 |
  • Eng
  • news title separator SLAMTEC Showcases at FAIR plus 2026, Debuts Four-Wheel Independent Steering Omnidirectional Platform, Igniting the Event with Full-Stack Embodied Intelligence Technologies

    fair plus banner
    FAIR plus 2026, the premier robotics industry event, brought together over 500 leading companies across the entire industrial chain and tens of thousands of professional visitors. The exhibition focused on the deep integration of AI and robotics, spotlighting the cutting edge of embodied intelligence, and building a world-class platform for technology exchange and industrial collaboration.
    fair plus crowd at the scene
    As a benchmark company in the embodied intelligence field, SLAMTEC was invited to participate. On this global stage of cutting-edge innovation, SLAMTEC centered its exhibition around "Embodied Intelligence,"presenting an integrated suite of technologies and products spanning perception → decision-making → motion, becoming one of the highlights of the event.

    A Real-World Answer to the Embodied Intelligence Wave

    At FAIR plus 2026, technology moved beyond concepts into tangible demonstrations.
    Through dynamic demos, system explanations, and hands-on experiences, SLAMTEC broke down embodied intelligence into a clear and practical pathway:
    • How robots understand space (Perception)
    • How they make decisions (Decision-making)
    • How they execute actions (Motion)
    The Aurora S 3D Localization & Mapping AI Spatial Perception System provides robots with stable, precise, and real-time 3D spatial understanding. During the event in Shenzhen, Aurora S performed live mapping, showcasing spatial perception and autonomous localization/navigation in a visible and verifiable way, attracting significant attention.
    aurora live mapping
    At the booth, SLAMTEC's full lineup of LiDAR products, along with flagship solutions such as the 48V Hermes embodied intelligent robot platform, drew continuous crowds from robotics companies, research institutions, and developer communities.
    SLAMTEC CEO Shikai Chen was interviewed by official event media and demonstrated the real-time mapping capabilities of the Aurora S system on-site.
    Interview CEO Chen Shikai
    Another major highlight was the offline debut of the Poseidon series four-wheel independent steering omnidirectional platform, which received strong recognition and enthusiastic feedback from the industry.

    Offline Debut | Poseidon Omnidirectional Platform

    At this exhibition, SLAMTEC officially unveiled the Poseidon Series Four-Wheel Independent Steering Omnidirectional Embodied Robot Platform.
    poseidon 1
    Designed specifically for embodied intelligence and humanoid robots, Poseidon directly addresses long-standing industry challenges:
    • Long development cycles
    • Limited payload capacity
    • Weak adaptability across scenarios
    • Insufficient operational stability
    The upcoming Poseidon series represents a major leap forward, combining innovative hardware architecture with full-stack software capabilities, setting a new industry benchmark.
    Key Highlights of the Poseidon Series:
    poseidon2
    • Zero-radius omnidirectional mobility: Flexible movement in complex environments with true in-place rotation
    • Ultra-low center of gravity design: Enhanced stability and safety
    • Full-stack SLAM navigation: Autonomous localization and path planning
    • 48V high-current power system: Supports high-power equipment
    • 360° multi-sensor fusion: Improved environmental perception
    • Up to 150 kg payload capacity: Expands industrial and research applications
    The platform supports a wide range of applications, including humanoid robot development, industrial logistics, campus inspection, and research/education—making it an ideal mobility solution for next-generation embodied robots.

    Sensor Fusion Driving Embodied Intelligence

    During a roundtable discussion at the event, SLAMTEC CEO Shikai Chen shared insights into perception technologies for humanoid robots:
    CEO Chen Shikai Speech
    1. Rejecting single-sensor approaches Humanoid robots should not rely solely on vision or stick to traditional LiDAR-only solutions. SLAMTEC advocates a multi-sensor fusion approach rather than following a single technical path.
    2. Solid-state evolution of LiDAR LiDAR is rapidly transitioning from mechanical to solid-state. The industry is now focusing on SPAD array chips, an area where SLAMTEC has already established technical groundwork. Meanwhile, LiDAR solutions for indoor wheeled robots remain stable and widely adopted.
    3. Deep fusion of LiDAR and vision as the mainstream Embodied intelligence and humanoid robots will be primarily vision-driven, complemented by deeply integrated solid-state LiDAR. Combined with large models and end-to-end SLAM, tightly coupled LiDAR-vision fusion is the long-term direction.
    4. Long-term investment in dual technology paths Since 2025, SLAMTEC has been developing both VSLAM and visual sensors. With a complete visual solution already launched, the company continues to advance both LiDAR and vision technologies in parallel.

    Moving Forward Together to Shape the Future of Embodied Intelligence

    Perception defines direction; mobility enables reach.
    With fully self-developed technologies in spatial perception, autonomous mobility, and intelligent navigation, SLAMTEC has built a complete link between a robot's brain (perception) and body (movement), delivering a one-stop core solution for embodied intelligence.
    slamtec products
    The successful showcase at FAIR plus 2026 highlights SLAMTEC's solid expertise and steady progress in AI spatial perception and embodied robot mobility platforms.
    Looking ahead, SLAMTEC will continue to drive innovation and product evolution, empowering the global embodied intelligence industry with core technologies—and bringing China's advanced robotics innovations to the world.

    关键字:Exhibition News

    top
    FaceTime Icon