When robots begin to truly "understand the world,"
the competition for next-generation intelligence is shifting from the "brain" to Perception + Action.
From April 22–24, 2026,
SLAMTEC will showcase at FAIR plus 2026,
presenting integrated technologies and products spanning Perception → Decision → Motion, centered on Embodied Intelligence.
📍 Booth: H9B20
📍 Location: Shenzhen Convention & Exhibition Center (Futian)
Aurora S 3D Localization & Mapping Perception System
Provides robots with stable and precise spatial understanding capabilities.
A live demo will be presented on-site, making it clear how perception drives action.
Key Specifications:
Mapping area: > 1,000,000 m²
Accuracy: ±5 cm
Weight: 238 g
Localization mode: VSLAM + LiDAR fusion
Global relocalization: Supported
Map management: Resume / Load / Save
Camera: Dual fisheye, FOV 180°
AI scene recognition: 18 outdoor scenes + 80 indoor scenes
Anti-interference capability: >90% detection rate in strong light / low-texture environments
For full technical specifications (including mechanical dimensions, frame rate customization, sensor synchronization, etc.), please visit us on-site or contact us for more information.
Multiple high-performance LiDAR products
48V Hermes embodied intelligence robotic platform
A new embodied robotic platform product will also be launched at the exhibition,
offering more flexible mobility for complex environments.
Perception drives action.
Slamtec looks forward to meeting you at FAIR plus 2026.
关键字:Exhibition News
Meet at FAIR plus 2026 | SLAMTEC Invites You to Explore the Future of Embodied Intelligence
Slamtec Shines in Tokyo! Empowering Global Robotics with Fully Integrated Spatial Perception
Event Recap | Slamtec & CIOE 2025 Successfully Concluded
Making a Bold Entrance at the 2025 World Robot Conference: SLAMTEC’s Four New Products Lead the New Era of Embodied Intelligence