메인
제품 센터 제품 센터
응용 사례
뉴스 동향
구매 채널
다운로드 및 지원
회사 소개
생태계 협력
연락처
메인
제품 센터 제품 센터
뉴스 동향
구매 채널
다운로드 및 지원
회사 소개
加入我们
연락처
  • 한국어 |
  • Eng
  • news title separator RPLIDAR U1: Consumer-Grade Underwater LiDAR Officially Launched

    Slamtec is proud to announce the release of the RPLIDAR U1, the industry’s first consumer-grade underwater LiDAR. With this launch, the underwater world is finally stepping into the era of high-precision LiDAR SLAM navigation.U1banner

    Compact Design for Consumer Applications

    Underwater LiDAR has been researched for years, but existing systems have been bulky, expensive, and unsuitable for consumer or commercial use.

    The RPLIDAR U1 changes this. Roughly the size of a ping-pong ball, it is compact enough to integrate easily into a wide range of devices. Even more importantly, Slamtec’s innovative system design makes it affordable for consumer and commercial applications.

    u1 size

    More Than Just Waterproof: A New System Architecture

    You might think waterproofing a LiDAR is enough—but it’s not.

    In water, traditional LiDARs face shortened detection range, noisy data, and poor accuracy, which is why sonar has remained the dominant tool for underwater detection. However, sonar lacks the precision required for SLAM-based underwater mapping and navigation.

    The RPLIDAR U1 solves this challenge with a completely redesigned ranging system, enabling stable underwater LiDAR scanning.

    • Waterproof rating: IPX8 (up to 5 meters depth)

    • Maximum detection range underwater: 5 meters

    With this breakthrough, underwater robots can now achieve the same high-precision mapping and navigation that LiDAR provides on land.

    Tested and Validated in Harsh Environments

    The underwater environment presents unique challenges:

    • Different water qualities

    • Reflective or absorbing surface materials

    • Strong sunlight interference

    The RPLIDAR U1 has undergone extensive testing to ensure reliable performance under all these conditions. Whether it’s murky water, pool environments, or coastal zones, the U1 consistently delivers accurate and robust LiDAR scans.

    u1sunlight test

    Powered by SLAMKIT: Complete Underwater Mapping & Navigation

    To accelerate development, Slamtec also provides the SLAMKIT Underwater Edition, a dedicated mapping and navigation solution designed to work seamlessly with the RPLIDAR U1.

    • No odometry required

    • Supports real-time mapping, localization, and navigation

    • Ready for integration into underwater robotics projects

    This ensures that developers and businesses can deploy underwater autonomous navigation solutions more efficiently than ever before.

    slamkit

    Example Applications of RPLIDAR U1

    The launch of RPLIDAR U1 opens up a wide range of consumer and commercial use cases:

    • Coastal vegetation exploration

    • Swimming pool cleaning robots

    • Underwater safety inspection & obstacle avoidance

    • Seabed exploration and research

    With its compact size, affordability, and precision, the U1 brings LiDAR-based autonomy to underwater environments.

    Conclusion

    The RPLIDAR U1 is more than just a new sensor—it is the beginning of the consumer-grade underwater LiDAR era. By combining compact hardware, affordable pricing, and Slamtec’s proven SLAM technology, the U1 enables a new generation of underwater robots, drones, and exploration devices.

    As the first of its kind, it will redefine how we map, navigate, and explore underwater worlds.

    关键字:rplidar

    top
    문의하기 버튼
    지원 이메일 버튼
    WhatsApp 버튼